ServerInfoService Service
You have created a service.
To test this service, you will need to create a client and use it to call the service. You can do this using the svcutil.exe tool from the command line with the following syntax:
svcutil.exe https://sdrswsdev.rockwellautomation.com/ServerInfo.svc?wsdl
You can also access the service description as a single file:
https://sdrswsdev.rockwellautomation.com/ServerInfo.svc?singleWsdlThis will generate a configuration file and a code file that contains the client class. Add the two files to your client application and use the generated client class to call the Service. For example:
C#
class Test { static void Main() { ServerInfoServiceClient client = new ServerInfoServiceClient(); // Use the 'client' variable to call operations on the service. // Always close the client. client.Close(); } }
Visual Basic
Class Test Shared Sub Main() Dim client As ServerInfoServiceClient = New ServerInfoServiceClient() ' Use the 'client' variable to call operations on the service. ' Always close the client. client.Close() End Sub End Class